DUG_Smoke alarm AC_WH-03

Checking the device history

Using the Wiser Home app, you can view the smoke and high temperature detection by accessing the smoke alarm history.
NOTE: All device history is stored in the cloud. When the cloud connection is lost, the device history will disappear.
  1. On the Control tab, tap All devices or a room tab where the Smoke Alarm is located.
  2. On the device control panel page, tap History.
    In the History page, you can see the date, time, and type of alarm detected.
    NOTE: Device history can be stored for a maximum duration of 90 days.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?