DUG_Smoke alarm AC_WH-03

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your smoke alarm with the Wiser Hub.
IMPORTANT: Do not mount the smoke alarm before pairing. The Setup/Reset button and power switch are located on the rear side of the smoke alarm.
NOTE: When multiple smoke alarms are paired with the same Wiser Hub, a radio frequency (RF) interconnection is automatically created between smoke alarms.
  1. Locate the power switch on the rear side of the smoke alarm. Use a screwdriver to turn the power switch to ON position.

    NOTE: When the smoke alarm is mounted on a wall or on the ceiling, the power switch is automatically turned ON.
  2. On the Home screen, tap .
  3. Tap Devices > > Safety and Security > Smoke Alarm.
    TIP: You can also navigate by tapping Control > > Safety and Security > Smoke Alarm.
  4. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the smoke alarm.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the smoke alarm manually and proceed to step 5.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

  5. Tap Next, short press the Setup/Reset button 3 times and make sure that the LED blinks amber.

    Wait for a few seconds until the LED turns green and the app confirms that the smoke alarm has joined.

  6. Tap Next and assign the device to a new room or an existing room and tap Submit.
    IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.

    After you pair the smoke alarm, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added sensor on the Control tab under the All and Room tabs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?