DUG_Fan Regulator-01

Adding a user

The Manage Users menu allows you to add new users and grant them access to devices or actions linked with your Wiser account.
  1. Tap Settings.
  2. Tap Manage Users.
  3. Tap Add User.
  4. Enter a Username and Email ID.
  5. Tap Access time and select any one of the following options from the dropdown menu:
    • From and To: Allows you to select a specific time and date.

    • Permanent: Allows you to select a permanent access.

    NOTE: Enter a date and time when selecting From and To.
  6. Tap Add location.
    The Select Location page appears.
  7. Select any of the listed locations and tap Add.
    TIP: You can select multiple locations and provide respective access levels.
  8. Select the access level (A) for the location from the following options:
    • No access: You do not have any permission to control the device.

    • View access: This allows you to view the devices.

    • Control access: This allows you to control the device.

    NOTE: When you select No access, you cannot choose a device from the devices list.
    TIP: You can also set the access level for Security (C).
  9. Select at least one device from the Devices (B) list.
  10. Tap Add User.
    An e-mail will be sent to the specified e-mail address.
  11. Tap Done.
    You have successfully added the new user. Now, you can see the new user on the Manage Users page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?