DUG_Fan Regulator-01

Switching On/Off the device using the app

By using the Wiser app, you can switch on/off the device.
To switch the device on/off:
  1. On the Devices page, tap Devices.
  2. Tap the power button (A) to switch on/off.
  3. You can also switch on/off from the control panel by tapping the power button (B) and adjust the fan speed by tapping the speed control options (C).
  4. Alternately, you can also switch on/off from the Dashboard page when you add a device to the favourites list.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?