DUG_Fan Regulator-01

Switching On/Off the device manually

You can switch on/off the device manually. The device will provide power to the electrical appliance connected to it.
Short press the push button on the device once to switch on/off the Fan Regulator.

You can press the up (A) and down (B) arrow buttons to increase and decrease the fan speed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?