48049-137-06EN

Graphic Display Navigation

Graphic Display Navigation Buttons

Graphic Display Screen

Display

The graphic display (A) functions if the trip unit is connected to a 24 Vdc external power supply or there is 150 V on at least two phases. Current alone (from primary injection test set or electrical system) will power the LSIG protection functions, but will not power the display.

Navigation buttons (B):

Metering Menu Button—Provides access to metering menus

Maintenance Menu Button—Provides access to maintenance menus

Protection Menu Button—Provides access to protection menus

Down Button—Moves cursor downward or decreases setting value

Up Button—Moves cursor upward or increases setting value

Enter Button—Selects an option from a list or enters the set values

Bar Graph Display and Menus

Menus

The MicroLogic P trip unit has a default bar graph display of currents and three different menus which can be accessed using navigation buttons:

A Bar Graph Display—Provides real-time bar graph display of line currents and measurement of line current and neutral current (if applicable) (default display)
B Metering Menu—Provides access to metered values of current, voltage, power, energy and frequency
C Maintenance Menu—Allows user to change the trip unit configuration and provides access to history logs
D Protection Menu—Allows precision adjustments to basic and advanced protection

When the switch cover is closed, the trip unit will return to the bar graph (default) display after 3.5 minutes of no input. (If the switch cover is open, the display stays at the window selected.) To access another menu, press the button that corresponds to the desired menu. The menu appears on the display and the green LED below the menu button lights up.

Metering Menu

Use the metering button to access the metered values of:

A Current
B Voltage
C Power
D Energy
E Frequency

Metering Menu

Current

Current Levels

Voltage

Voltage Levels

Power

Power Levels

Energy

Energy Levels

Frequency

Frequency Levels

Maintenance Menu

Use the maintenance button to access the maintenance menu.

A To access the history log
B To set up the M2C/M6C contacts
C To set up the MicroLogic trip unit
D To set up the metering parameters
E To set up the communication module

Maintenance Menu

History Logs

History Logs

M2C/M6C Programmable Contacts

M2C/M6C Contacts Setup

  • Available only if M2C/M6C contacts are installed.

  • One alarm per contact.

  • Can select those set up as “alarm” or “trip” under protection menu.

MicroLogic Setup

MicroLogic Setup

NOTE: If trip unit is connected to a communication network which provides date and time synchronization, date/time cannot be set from trip unit.

Metering Setup

Metering Setup

Communication Setup

Use the metering button to access the metered values of:

A Current
B Voltage
C Power
D Energy
E Frequency

Metering Menu

Protection Menu

Use the protection button to access the menus.

A To display and adjust current protection
B To display and adjust voltage protection
C To display and adjust other protection
D To set current load shedding
E To set power load shedding

Protection Menu

Amperage Protection

Amperage Protection

Voltage Protection

Voltage Protection

Other Protection

Other Protection

Current Load Shedding

Current Load Shedding

Power Load Shedding

Power Load Shedding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.