48049-137-06EN

Trip Unit Replacement

Trip unit replacement must be done by qualified persons, as defined by the National Electric Code, who are familiar with the installation and maintenance of power circuit breakers.

Before replacing trip unit, confirm that the circuit breaker is in good working condition. If the condition of the circuit breaker is unknown, do not proceed. For assistance in evaluating the condition of the circuit breaker, call Technical Support.

Read this entire section before starting the replacement procedure.

If trip unit being replaced is a MicroLogic 2.0, 3.0 or 5.0 trip unit, order connector block S33101 and circuit breaker or cradle wiring harness if necessary.

DANGER
hazard of electric shock, explosion, or arc flash
  • Failure to follow these instructions for installation, trip test and primary injection testing may result in the failure of some or all protective function.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, NOM 029-STPS or local equivalent.
  • Replacement/upgrading of a trip unit in the field must be done by qualified persons, as defined by the National Electric Code, who are familiar with the installation and maintenance of power circuit breakers.
  • Before replacing/upgrading trip unit, confirm that the circuit breaker is in good working condition. If the condition of the circuit breaker is unknown, do not proceed. For assistance in evaluating the condition of the circuit breaker, call Technical Support.
  • If the circuit breaker fails to function properly in any manner upon completion of the trip unit installation, immediately remove the circuit breaker from service and call Field Services.
  • Turn off all power supplying this equipment before working on or inside equipment. Follow instructions shipped with circuit breaker to disconnect and reconnect circuit breaker.
  • Replace all devices, doors and covers before returning equipment to service.
Failure to follow these instructions will result in death or serious injury.

Required Tools

  • Torque-controlled screwdriver, set at 7 in-lbs (0.8 N•m) ± 10% (Lindstrom torque driver MAL500-2 or equivalent)

  • The appropriate MicroLogic test kit found in Section 7 of The Digest (Reference 0100CT1901).*

Preparation

Record Switch Settings

Record all trip unit switch and advanced protection settings for later use.

Circuit Breaker Disconnection

Disconnect circuit breaker as directed in the circuit breaker instruction bulletin shipped with the circuit breaker. The circuit breaker must be completely isolated. (For a drawout circuit breaker, place circuit breaker in the disconnected position. For a fixed-mounted circuit breaker, all voltage sources, including auxiliary power, must be disconnected.)

Circuit Breaker Accessory Cover Removal

Remove circuit breaker accessory cover as directed in the Install Accessories section of the circuit breaker instruction bulletin shipped with the circuit breaker.

Rating Plug Removal

A small Phillips screwdriver is needed to remove the adjustable rating plug.

  • Open switch cover (A).

  • Unscrew adjustable rating plug mounting screw (B).

  • Remove adjustable rating plug (C). Save for installation in replacement trip unit.

Remove Adjustable Rating Plug

Trip Unit Removal

  1. Remove connector block (A) from top of trip unit, if present.

  2. Loosen two trip unit screws (B).

  3. Slide out trip unit (C).

Remove Existing Trip Unit

Trip Unit Replacement

Battery Installation

Install Battery

 

Trip Indicator Lights

If a new trip unit is being installed, install the trip unit battery.

Install battery holder with battery (A) in trip unit, observing the correct polarity as indicated on the battery compartment.

NOTE: Battery holder with battery is located under the side flap in the cardboard box the trip unit is shipped in.






Press test/reset button (A). All four indicator lights (B) should light. If they do not light, check polarity of battery and retest. If indicator lights still do not light up when test/reset button is pressed, stop installation and contact the local sales office for factory authorized service

Trip Unit Installation

  1. Inspect trip unit connector pins and surfaces. If there is any damage, misaligned pins, or contamination, stop installation and contact the local sales office for factory authorized service.

  2. Inspect trip unit mounting base on the circuit breaker. Clear any debris from area and check that all accessory wiring is properly routed for the trip unit being installed. If there is any damage or contamination, stop installation and contact the local sales office for factory authorized service.

  3. For MasterPacT NW circuit breaker only: Manually depress trip unit interlock (A) and hold it in place during steps 4–6 below.

  4. Align guide rail (B) on bottom of trip unit with guide rail slot (C) on trip unit mounting base in circuit breaker and gently slide the trip unit in until it stops.

    NOTE: The MasterPacT NT and NW trip unit mounting bases are shock mounted and therefore can flex slightly.

    Install Trip Unit

    CAUTION
    Hazard of equipment damage
    Check installation of trip unit to assure proper connections and seating.
    Failure to follow these instructions can result in injury or equipment damage.
  5. Align the trip unit so top mounting screw (A) aligns with the top threaded insert and start the screw by turning the screw two full rotations.

  6. Use a torque-controlled screwdriver to drive the bottom screw (B) to 7 in-lbs. (0.8 N•m) ± 10%. The back of the trip unit must be flush with the trip unit mounting base.

  7. Use a torque-controlled screwdriver to drive the top screw to 7 in-lbs. (0.8 N•m) ± 10%. Mounting tab must be flush with the mounting standoff and sensor plug.

    NOTE: The face of the closed switch cover must be flush with adjoining mounting base surfaces. If these surfaces are not flush, stop installation and contact the local sales office for factory authorized service.
    NOTE: If you are upgrading from a MicroLogic 2.0, 3.0 or 5.0 trip unit, the connector block must be ordered separately (Part Number S33101). See instructions shipped with the connector block for installation into circuit breaker.
  8. Install connector block (C) into top of trip unit.

    Secure Trip Unit

  9. Install adjustable rating plug into the trip unit.

    a. Open switch cover (A) on new trip unit.

    b. Inspect mounting area for debris and contamination.

    c. Gently push adjustable rating plug (B) into new trip unit.

    d. Tighten adjustable rating plug mounting screw (C). The plug will be drawn into position flush with front face as screw is tightened.

  10. Set trip unit switches and advanced protection settings to values recorded above or per coordination study results.

  11. Close switch cover (A).

    Install Adjustable Rating Plug

Circuit Breaker Accessory Cover Replacement

Replace circuit breaker accessory cover as directed in the Install Accessories section of the circuit breaker instruction bulletin shipped with the circuit breaker.

Trip Unit Installation Check

Secondary Injection Testing

Field installation of a trip unit requires secondary injection testing with an appropriate test kit. This will ensure that the newly-installed trip unit is functioning properly. The test will require opening and closing the circuit breaker. Follow the procedures outlined in the instruction bulletins shipped with the circuit breaker and the test kit.

  1. Make sure the circuit breaker is isolated from all upstream and downstream devices.

  2. Perform secondary injection testing as outlined in the instruction bulletin shipped with the test kit. Verify that all applicable trip unit functions are operating properly.

  3. If any test fails, do not put the circuit breaker into service and contact the local sales office for factory authorization service.

Primary Injection Testing

Primary injection testing is recommended to ensure that all trip system connections have been correctly made. Perform primary injection testing per the instructions in the Field Testing and Maintenance Guide, bulletin 48049-900-xx, where xx is 02 or higher.

Check Accessory Operation

  1. Installed accessories – Validate the proper operation of all installed accessories. See the corresponding accessory instruction bulletins for operational testing procedures.

  2. Programmable contact module – If circuit breaker has an M2C or M6C programmable contact module installed, validate its proper operation. See the corresponding accessory instruction bulletins for operational testing procedures.

  3. Zone selective interlocking – If the circuit breaker is part of a ZSI system, follow the zone selective interlocking test procedures as outlined in the appropriate test kit instruction bulletin.

  4. Communications – If communication modules exist, confirm circuit breaker has re-established communications with the supervisor.

Trip Unit Setup

  1. If an auxiliary power supply is being used for the MicroLogic trip unit, reconnect the auxiliary power supply.

  2. Reset the trip unit switches and advanced protection settings to original values, as recorded at the beginning of this section.

Circuit Breaker Reconnection

Reconnect circuit breaker as directed in the circuit breaker instruction bulletin shipped with the circuit breaker.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.