48049-137-06EN

Operation

Metered Values

Metering Menu

Use the metering menus to monitor circuit breaker current (I), voltage (V), power (P), energy (E) and frequency (F).

NOTE: System measurements can also be checked remotely using System Manager Software (SMS) (version 3.3 or later) or other network system management software.

Current Levels

Ia Instantaneous A phase current

Maximum measurements can also be reset to zero.

Check Current Levels

Ib Instantaneous B phase current
Ic Instantaneous C phase current

In

Instantaneous neutral current
Instantaneous ground current

Iamax

Maximum instantaneous A phase current
Ibmax Maximum instantaneous B phase current
Icmax Maximum instantaneous C phase current
Inmax Maximum instantaneous neutral current
Maximum instantaneous ground current
Voltage is above set maximum
Demand B phase current

Demand C phase current

Demand neutral current
Maximum demand A phase current
Maximum demand B phase current
Maximum demand C phase current
Maximum demand neutral current

Voltage Levels

   

Check Voltage Levels

Vab Instantaneous voltage between A and B phases
Vbc Instantaneous voltage between B and C phases
Vca Instantaneous voltage between C and A phases
Van Instantaneous voltage between A phase and neutral
Vbn Instantaneous voltage between B phase and neutral
Vcn Instantaneous voltage between C phase and neutral
   

Power Levels

P Instantaneous active power
NOTE: To ensure reliable power and power factor measurements, Set Power Sign, and Set Sign Convention.

Check Power Levels

Q Instantaneous reactive power
S Instantaneous apparent power
Power Factor Instantaneous power factor
Demand active power
Demand reactive power
Demand apparent power
Maximum demand active power
Maximum demand reactive power
Maximum demand apparent power
Maximum measurements can also
be reset to zero.
   

Energy Levels

Total active energy (P)
NOTE: To ensure reliable energy measurements, Set Power Sign, and Set Sign Convention.

Check Energy Levels

Total reactive energy (Q)
Total apparent energy (S)
Active energy in (E.P.)
Reactive energy in (E.Q.)
Active energy out (E.P.)
Reactive energy out (E.Q.)
Energy measurements can also
be reset to zero.

Frequency

Check Frequency

Trip Unit History

Use the maintenance menu to review the trip unit history stored in the history logs.

History Log Menu

Trip History

The trip unit stores information about the LSIG fault causing the last ten trips. For each fault the following are stored:

  • Current values of Ir, Isd, Ii, and Ig

  • Pickup setpoint for voltage and other protection

  • Date

  • Time (hour, minute and second)

NOTE: Trips from use of a test kit are not recorded in the trip history log.

Check Trip History

Alarm History

The trip unit records measurement at each of the last ten alarms activated. For each alarm the following are stored:

  • Indication and value of the alarm setting

  • Date

  • Time (hour, minute and second)

Check Alarm History

Operation Counter

This displays the maximum number of operations (trip or circuit breaker openings) since the circuit breaker was installed. The number is obtained from the circuit breaker communication module (BCM).

Check Operation Counter

Contact Wear

This displays the amount of contact wear on the contact with the greatest wear. When this number reaches 100, it is recommended that a visual inspection of the contacts be done. This function works only on MasterPacT NT and NW circuit breakers.

Check Contact Wear

Protection Setup

Use the protection menus to check protection setup for amperage protection, voltage protection, other protection, current load shedding and power load shedding.

Refer to Appendix B for default settings and setting ranges.

Protection Menu

Amperage Protection

The “Change Idmtl (A) setting with I(A)” screen will only appear if long-time, short-time and/or instantaneous adjustments have been previously made under the Idmtl (A) menu screen. If the user responds Yes, the Idmtl (A) settings will be lost when the menu goes to the I(A) adjustment screen. If no adjustments have been made under the Idmtl (A) menu screen, the menu goes directly to the I(A) adjustment screen.

The “Change I (A) setting with Idmtl(A)” screen will only appear if long-time, short-time and/or instantaneous adjustments have been previously made under the I(A) menu screen. If the user responds Yes, the I(A) settings will be lost when the menu goes to the Idmtl(A) adjustment screen. If no adjustments have been made under the Idmtl(A) menu screen, the menu goes directly to the I(A) adjustment screen.

NOTE: Neutral protection is disabled if Idmtl protection is selected.

Check Amperage Protection

Check Amperage Protection

NOTE: Selection of the CT type determines the Ineutral protection in the Protection menu.
Circuit Breaker Neutral CT Type Protection Choices
All none disabled
Four-pole internal OFF: no neutral protection
N/2: half neutral protection
N: full neutral protection
Three-pole external OFF: no neutral protection
N/2: half neutral protection
N: full neutral protection
1.6N: oversized neutral protection

Check Amperage Protection

NOTE: To set Inmax, the neutral CT must be set to external or internal under MicroLogic setup under the maintenance menu.

Voltage Protection

NOTICE
Hazard of equipment damage
Setting undervoltage protection (Vmin) below 80% or voltage unbalance (Vunbal) above 20% can cause the trip unit to not perform as expected.
Failure to follow these instructions can result in equipment damage.

Voltage protection pickup settings are phase-to-phase values.

Unbalance values are based on the true RMS values of the three-phase currents.

Undervoltage alarm drops out upon the loss of the second phase.

NOTE: Do not set undervoltage protection below 80%. Do not set Vunbal above 20%*

Check Voltage Protection

Other Protection

Check Other Protection

Current Load Shedding

Current load shedding can be configured for alarm only. It cannot be used to trip the circuit breaker.

Check Current Load Shedding

Power Load Shedding

Power load shedding can be configured for alarm only. It cannot be used to trip the circuit breaker.

NOTE: Press Protection button to view Protection Menu.

Check Power Load Shedding

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.