80043-868-01

Install NF Sub-feed Circuit Breaker Interior Inside the Enclosure

DANGER
hazard of electric shock, explosion, or arc flash
Replace all devices, doors, and covers after installing this kit and before turning on power to the equipment.
Failure to follow these instructions will result in death or serious injury.
  1. Install the Interior into the enclosure as instructed in NF/NFOM Panelboards User Guide (document number 80043-741) stated in section “Interior Mounting for Square D Brand Enclosures”.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?