Fiber Manager Schematics

You can use Fiber Manager to generate three types of schematics:

  • Circuit schematics show a graphical representation of a given circuit.

  • Fiber trace schematics show a graphical representation of any trace you create.

  • Splice schematics show a graphical representation of all connections within a given splice point.

Fiber Manager bases its schematics functionality on ArcMap's Schematics extension. You can find more Schematic command information in the ArcGIS help. While splice and circuit schematics require schematic configuration by your administrator, fiber trace schematics require only the classic or flexible Fiber Manager configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.