Change Only the Wavelength on a Circuit

You can change only the wavelength on a circuit and leave the header untouched.

  1. Open Circuit Manager and locate the circuit.
  2. Type a value in the Wavelength field then click off the field.
  3. Click the Create Fiber Path Trace Report checkbox and then click Trace.
  4. Verify that the top of the report reflects the wavelength change you made.
  5. Click Save to save your changes, then click Close to exit Circuit Manager.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.