Using Circuit Manager

A circuit is a veritable path. You can create a circuit for a glass path without distinguishing the wavelengths that travel along that path. Or you can create a separate circuit for each wavelength on a glass path. Circuit Manager helps you:

  • Create and edit circuits associated with an end-to-end path in the fiber network

  • View and manage circuit information

  • Define and edit circuits along a connected path

  • Change the header (origin) of a circuit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.