Circuit Schematics

Circuit schematics show a graphical representation of one or more circuits. Perform the following steps to create a schematic.

  1. Enable the Schematics extension and the Schematic toolbar.
  2. Open a Stored Display.
  3. On the Schematic toolbar, click the Generate New Schematic Diagram button to open the New Schematic Diagram window.
  4. Select a schematic dataset or folder from the drop-down menu, or use the browse icon to search for the dataset or folder.
  5. Select a schematic diagram template. Available templates vary according to your configuration.
  6. Select [Create New Data Frame] from the Output Data Frame drop-down menu.
  7. Type a name for the schematic diagram and click OK.
  8. Select one or more circuits from the list. You can use the Shift and Ctrl keys to select multiple circuits. Click Export. A schematic diagram displays in the map window.
    TIP: It may take a few minutes for this step to complete if this is the first time you've exported this circuit.
  9. Use standard ArcMap view commands to view the schematic. The schematic diagram is displayed with the symbols and text options defined by your system administrator.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.