Sending Multiple Messages
You may send multiple messages in one URI request. For example, the following request sends two messages to ArcFM Mobile in a single URI:
//Opens ArcFM Mobile, sets the World Street Map basemap, and selects the Schneiderville Electric operational map
arcfmmobile:?basemap=a%20World%20Street%20Map&operationalmap=Schneiderville%20Electric
Here’s an example of several messages being sent in one URI:
//Opens ArcFM Mobile at this lat/long, at this zoom scale, changes the basemap to World Imagery, and changes the operational map to Schneiderville Electric
arcfmmobile:?lat=29.678&long=-82.373&scale=1500&basemap=World%20Imagery&operationalmap=Schneiderville%20Electric
The query aspect of the URI must be key=value, so lat=29.659 and long=82.354 are
examples of proper query syntax. If you launch URI requests inside
a batch file or using a command line, the ampersands must be escaped
with a caret (^), as shown here:
//Opens ArcFM Mobile at this lat/long, at this zoom scale, changes the basemap to World Imagery, and changes the operational map to Schneiderville Electric
arcfmmobile:?lat=29.678^&long=-82.373^&scale=1500^&basemap=World+Imagery^&operationalmap=Schneiderville+Electric
Here are a few items to keep in mind for constructing commands:
-
Each space character must be replaced by the plus (+) symbol.
-
Location coordinates must be in the format
123.456with a period and never a comma. -
A question mark (?) is required after the first colon (:) to mark where the parameters start.
-
Parameters can be specified in any order.