Work Location (wl) Key
wl) key places a work
location graphic on the map and zooms to it at the given coordinates.
It can optionally include a label, be associated with specific markup
types, and be associated with an existing as-builting job. Multiple
work locations can be included in a single URI command.| Parameter | Description | Important Considerations |
|---|---|---|
lat and long
|
These parameters specify the position of a work location (wl) on the map. |
|
label
|
When provided, the given label is placed next to the work location graphic on the map. |
|
markupTypeID
|
One or more markupTypeID parameters may be
included for any one wl key, but each must have a
number associated with it (e.g. markupTypeId1, markupTypeId2, etc.). Each markupTypeID parameter given should equal an existing markup type globally unique
identifier (GUID) in your tenant. You can view each markup type's
GUID in the Mobile plugin in the Solution Center. |
|
wr
|
This allows you to associate a work location with an existing as-builting job. This parameter must equal the GUID of an existing work request that is associated with an as-builting job for the user. This parameter does NOT automatically open the as-builting job, rather it places a work location graphic in the map. The user can then tap it to open the as-builting job directly from the map. |
The |