Work Location to Open (wltoopen) Key
The wltoopen key automatically opens a markup
job at a work location graphic that is included in the same command,
rather than making the user tap on the work location to start a markup
job there.
-
IMPORTANT: This key is supported in iPad only and cannot be used to open an as-builting job. If you want to automatically open an as-builting job, you should use the
workrequestidkey. If you want a work location graphic as well, you can also place one with thewlkey and associate it with the as-builting job. -
This key must be equal to a label of a given
wlkey in the same command. -
Only one
wltoopenkey can be in any given command, and it can only start a markup job for one work location in the command. -
The markup job that is started using this command is automatically given the name equal to the label of the work location.
-
If a
workRequestIdis included as part of thewlkey, keep the following in mind:-
If one
markupTypeIdis provided and thewltoopenkey IS included in the command, the markup job is immediately started for that work location, and the palette for the designated markup type is automatically opened. -
If more than one
markupTypeIDis provided and thewltoopenkey IS included in the command, the user is prompted to pick one of the designated markup types. After they do this, the markup job is automatically started, and the palette for the chosen markup type opens.
-
Examples
//Opens the app, then opens a work location that does not have a markupType designated (user prompted to select markup type)
arcfmmobile:?wltoopen=WR854668756&wl=lat%3D29.655574%3Blong%3D-82.330221%3Blabel%3DWR854668756
//Opens the app, then opens a work location that has one markupType designated (user not prompted to select markup type)
arcfmmobile:?wltoopen=WR854668756&wl=lat%3D29.655574%3Blong%3D-82.330221%3Blabel%3DWR854668756%3Bmarkuptypeid1%3D928ab1ab-4611-436d-ae38-b1436f1fe674
//Opens the app, then opens a work location that has multiple markupTypes designated (user prompted to select one designated type)
arcfmmobile:?wltoopen=WR854668756&wl=lat%3D29.655574%3Blong%3D-82.330221%3Blabel%3DWR854668756%3Bmarkuptypeid1%3D928ab1ab-4611-436d-ae38-b1436f1fe674%3Bmarkuptypeid2%3D36ee0000-ffd8-0003-5ec7-08d833db7652