Tasks Button

The Tasks button can be configured for availability in ArcFM Mobile after a user identifies one or more assets in the map, also after a user performs a trace.

The following images show an example of the Tasks button after an Identify operation:

After tapping Tasks, the following examples are available, according to the .json provided in the iOS box:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?