Identify Assets at a Location

Publishes in WPF and Xam {Windows and iPad}, and profiled as such

To illustrate the way to identify an operational item, in the example below we identify a pole.

  1. WPF - the next step goes with this one
    Click the Identify button at the bottom right, then click on the pole in the map.
  2. WPF
    You can optionally draw a lasso in the map. We drew a rudimentary lasso for this example.

    Pins appear in the map and highlight the assets that are attached to the pole.

    The highlighted pins in the map correspond with the list of assets available on the Identify tab.

  3. WPF
    Click the View button to read more about the fuse. The fuse’s locator turns white and bounces in the map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.