Tasks

Publishes in Xam and Android, and WPF

Depending on the operational map you select, there are numerous possible tasks that you can perform relevant to the actions you are currently undertaking.

TIP: Your administrator has the ability to configure the options that are available when using this tool.

Identify Tasks

When you perform an Identify operation, after you tap the Tasks button at the top of the Identify pane, similar options to those in the following image may be available to you:

To view tasks for one asset, click the View button to the right of the asset, then click Tasks. You may see a menu similar to the following:


Tasks for tracing is not released yet. 4/12/22

Trace Tasks

When you perform a Trace operation, after you tap the Tasks button at the top of the Trace pane, you may have options available to you, as seen in the following image:






Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.