Maps
button on the left side of the app.
Online and offline maps alike display a scale in the lower, left-hand corner of the map, which updates as you zoom in and out..
View Different Maps
Icons next to each map in the list indicate if it contains components that are offline.
Basemaps are shown under the Backdrop tab.
Maps of facilities, parcels, and other searchable maps are shown under the Operational tab. Each operational map may contain offline and online data.
Click or tap once on a map to interact with it in the map pane.
If you are in offline mode, on the Operational tab, every online-only map is grayed out.
View Only Offline Maps
To view only
offline maps, click the offline mode
button.
Consider using this functionality if you are going to be working in
an area with poor internet connectivity, or if your organization is
trying to limit data plan consumption. When offline mode is selected,
performing a search or an identify returns results only from data
that has been downloaded.
A line through the button indicates that no online maps are available. All online maps disappear from the map and online-only maps are not selectable on the Map tab.
If you go back online and your device loses connectivity, the
icon toggles between online
and offline
.
To view only offline maps,
click the offline mode
button. Consider using this functionality
if you are going to be working in an area with poor internet connectivity,
or if your organization is trying to limit data plan consumption.
When offline mode is selected, performing a search or an identify
returns results only from data that has been downloaded.
When online mode is selected, the map display, search, and identify tools stream data from the map server. If the device loses connectivity while online mode is enabled, the app automatically switches to use offline data. In this case, the icon does not toggle from online to offline. When connectivity is re-established, the app automatically reverts to streamed data.