Attach Photos to Markups
In the following example, we place a callout next to a switch cabinet, attach photos of the transformer, and use the image editor to add helpful text plus some freehand drawing.
- Tap on the toolbar to add a callout in the map.
- In the Markups pane, tap the pencil edit button to rename the job as appropriate.
- To attach photos to the markup, tap the Camera icon, and select to take a picture or to view the gallery.
- Choose your photos and tap Add. The selected photos are attached to the markup, and circular dots under the photos indicate that more than one is attached.
Edit Photos
When you need to edit a photo, such as switch its orientation or add helpful text/arrows to aid in communication back to the office, select a photo to enlarge it and allow editing. Text, Drawing & Shapes, and Crop & Rotate tools are available underneath the photo.
- Tap Drawing & Shapes to access the freehand tools,
which allow you to draw whatever you want in the photo. First, select
the following settings for drawing:
After you move the opacity slider or the thickness slider, in the middle of the photo a dot briefly appears, representing the color, opacity, and thickness that you chose above.
- When you are finished with the above settings, tap to create your freehand drawing in the photo.
- Use the additional tools in the Drawing & Shapes menu
to aid in highlighting important aspects of the photo.
-
— place a square on the image and provides access
to the color picker, opacity, and thickness tools -
— place a circle on the image and provides access
to the color picker, opacity, and thickness tools -
— place a line or arrow on the image and provides
access to the color picker, opacity, and thickness tools
-
- Use the Text tool to add helpful information regarding elements in the photo. The following tools help you choose the settings for your text:
- Tap +Add and type the text you want displayed, then tap OK.
- The Crop & Rotate tools enable you to flip a photo
on its horizontal or vertical axis and crop out unnecessary parts.IMPORTANT:
-
If you need to crop, rotate, or flip the photo, use those tools prior to adding text, otherwise the text might end up reversed or upside down.
-
When you do perform an image transformation (crop/rotate/flip), the Undo operation is not available.
-
- Above the photo, tap Reset to remove all of your edits. Alternatively, use the undo/redo arrows to reset or redo edits one by one.
- Tap Save to save your edits to a photo.