Identify Assets at a Location

Publishes in WPF and Xam {Windows and iPad}, and profiled as such

To illustrate the way to identify an operational item, in the example below we identify a pole.

  1. MAUI- the next step goes with this one
    Tap the Identify button at the bottom right of the map, then tap on the pole in the map.
  2. MAUI
    You can optionally draw a lasso in the map. We drew a rudimentary lasso for this example.

    The list of assets within the area you draw displays under Identify, and the assets' corresponding locators appear in the map.

  3. MAUI
    Tap the right-facing arrow to view the conductor’s attributes. The conductor’s locator turns white and bounces in the map.

Publishes in Xam & MAUI
.
IMPORTANT: If your organization has configured custom tools for selected equipment, a Tasks button provides additional actions that differ based on what is configured for the identified results.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?