Add Fields and Model Names
To be able to control the order and width for components sharing the same rack slot, you need to add four fields to the fiber object tables that Wavepoint supports in the rack view. The four fields are not part of the standard sample data, which is why you need to add them before you can configure multiple components sharing a slot.
The four tables to update are:
-
F_ActiveDevice (in case your company changed the table name, it is the object table assigned the ACTIVEDEVICE class model name)
-
F_Device (or, the object table assigned the ENDDEVICE class model name)
-
F_PassiveDevice (or, the object table assigned the PASSIVEDEVICE class model name)
-
F_PatchPanel (or, the object table assigned the PATCHPANEL class model name)
The four fields and model names to add to the tables are:
|
Field Name |
Field Type |
Field Model Name |
Notes |
|---|---|---|---|
|
WavepointLayoutMode |
Short Integer |
WAVEPOINTLAYOUTMODE |
Determines the unit (inches, millimeters, or rack units) to use for the child devices’ widths. |
|
WavepointOrder |
Short Integer |
WAVEPOINTORDER |
Determines the objects’ position order within the slot from left to right. |
|
WavepointWidth |
Double |
WAVEPOINTWIDTH |
Determines the width of the child fiber object, respecting the unit chosen in the layout mode. |
|
WavepointHeight |
Double |
WAVEPOINTHEIGHT |
Not currently used, and is reserved for future use. To change height, configure the columns of the fiber object as described in Populate Required Rack, Device, and Port Fields. |
The following steps demonstrate how to accomplish this using the F_PatchPanel as its example.
- In ArcCatalog, sign into the geodatabase as the owner of the fiber object tables.
- In the Catalog Tree, locate the F_PatchPanel table.
- Right-click F_PatchPanel and choose Properties.
- On the Fields tab, scroll to the bottom of the field list
until you find the first empty row.IMPORTANT: If you do not see an empty row, it means you are either not signed in as the schema owner, or there are other users in the geodatabase causing the schema to be locked. Ensure you are signed in as the owner and that you have full ownership of the geodatabase while attempting to modify the schema.
- Add the following fields to the table:
- Click OK.
- Still in the Catalog Tree, right-click F_PatchPanel again and choose ArcFM Properties Manager.
- On the Field Model Names tab, assign the following field model names:
- Click OK.
- Repeat the steps above for the F_ActiveDevice, F_Device,
and F_PassiveDevice tables.IMPORTANT:
Because this is a schema change, you need to restart your ArcGIS Server and also restart your IIS Server on the server machine before overwriting your published service. If you attempt to re-publish your service without restarting ArcGIS Server and IIS Server, you receive the following message:
To correct this, restart ArcGIS Server and IIS Server, then overwrite the published service.