Install ArcFM Server

Install the latest version of ArcFM  Server on the machine from which you intend to host your map service.

IMPORTANT: Please visit myArcFM for the most up-to-date information about supported versions.

When the installation completes, a dialog appears allowing you to register the Server Object Extension (SOE). Instead of registering the SOE that enables Wavepoint through one of these commands, complete this in an upcoming configuration step.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?