Wavepoint Configuration Overview
Before You Begin
Ensure the computer you are using as the server has adequate hardware for the task. Only 64-bit environments are supported.
Choose Hardware Structure
There are four components to Wavepoint:
- 
               
The geodatabase, which is the source of data for a published web service
 - 
               
ArcMap/ArcFM to manage the underlying data and publish the web service
 - 
               
ArcGIS server to manage access to the service once published
 - 
               
The Wavepoint web application
 
You can choose between two supported hardware structures to host each of these four components:
- 
               
On a single machine
 - 
               
Separately on multiple machines
 
Client Machines Requirements
The client machines must run one of the following supported web browsers:
- 
               
Google Chrome
 - 
               
Mozilla Firefox
 - 
               
Internet Explorer 9 and above
 
Supported Versions
For a full list of supported versions and required licenses, visit the myArcFM page Wavepoint Supported - Versions.