Windows Server 2008 R2

The default IIS settings in Windows Server 2008 R2 should adequately support Wavepoint. Ensure you check which IIS features are installed.

  1. In the Start menu, right-click Computer and select Manage.
  2. In the Server Manager window's left menu, expand Roles.
  3. Click Web Server (IIS).
  4. In the Web Server pane, scroll down to the Role Services section.
  5. Ensure the following services are installed:

  6. If some services are not installed, use the Add Role Services button to the right of this pane to add them.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?