Search Field

The search field in Wavepoint searches the display field configured for each fiber feature class. For example, the following image shows four hits on the same search:


These search fields are chosen in the Layer Properties dialog > Display tab for each feature class and table:


We recommend choosing a relevant field that is usually populated with a unique name or identifier.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?