Start ArcGIS Server Service

After installing ArcGIS Server but before installing ArcFM applications, you stopped the ArcGIS Server service.

That service must be restarted before you can proceed to use ArcGIS Server Manager to add the Server Object Extension (SOE) that enables Wavepoint .

  1. Log into your server machine.
  2. Access the Services dialog:
    1. Press the Windows key and then type “Services” to find the dialog.
    2. Or, press Ctrl+Shift+Esc to open Windows Task Manager, and from there navigate to the Services tab.
  3. Right-click ArcGIS Server and choose Start.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?