DUG_Iconic Dimmer_CLP-00

About the device

The Iconic Connected Dimmer (hereinafter referred to as Dimmer) is a push-button device that can be used to switch and dim LED, ohmic, inductive or capacitive loads manually or remotely. It can detect the load automatically and provides thermal protection, overload-resistance and short-circuit protection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?