DUG_Iconic Dimmer_CLP-00

Setting timer mode

You can set the timer to turn off the device after a certain period of time.
In Wiser app, change the mode from switch to timer, refer to mode settings.
  1. On the device control panel page, tap timer (A) for the slide-up menu.
  2. In the slide-up menu select the required Set Period (B) and tap Save.
    NOTE: The timer mode will be stopped automatically at the end of the countdown timer. If the timer mode feature is enabled, and there are one or more Schedule/Moment/Automation actions in this period, then the system will stop the current mode action immediately, and perform the new actions (the new action always has a higher priority than the current action).
Once the countdown timer reaches zero, the device turns off.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?