DUG_Iconic Dimmer_CLP-00

Dimmer settings

Using The Wiser app, you can manage the Dimmer modes and settings.

To access the dimmer settings:

  1. On the Home page, tap All devices > Iconic Dimmer.

  2. On the device control panel page, tap Settings.

Dimming Range

You can restrict the minimum and maximum brightness of the load connected to the device. This is done to avoid flickering and switching off the LED.

Tap Dimming Range and do either or both of the following:

Minimum Brightness: drag the sliding bar to restrict the minimum brightness.

TIP: If you set the minimum brightness to the right most position on this sliding bar, then the load glows at the minimum brightness even if you drag the sliding bar to the lowest value in the control panel.

Maximum Brightness: drag the sliding bar to restrict the maximum brightness.

TIP: If you set the maximum brightness to the left most position on this sliding bar, then the load glows at the maximum brightness even if you drag the sliding bar to the highest value in the control panel.

Toggle mode setting

Using this setting, the device will remember the last state of the device.

Tap Toggle Mode Setting and select any one of the following:

100%: the LED glows at maximum brightness every time it is turned on.

Last Level (Memory Function): the LED glows at the previously set brightness level every time it is turned on.

LED Indicator Mode

You can select the LED indicator mode for easy identification of the device status.

Tap LED Indicator Mode and select any one of the following:

Reverse With Load: the LED on the Dimmer is on when the device is off.

Consistent With Load: the LED on the Dimmer is on when the device is on.

Always Off: the LED on the Dimmer is always off.

Always On: the LED on the Dimmer is always on.

For information on LED color during each modes, refer to LED indication.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?