DUG_Iconic Dimmer_CLP-00

Creating a schedule

Using a schedule, you can control and trigger the device. The system will follow the active schedule once it has been set. You can create or modify schedules at any time.
  1. On the Home page, tap All devices > Iconic Dimmer .
  2. Tap (A) to set the start time and tap (B) to set end time.
  3. Tap (C) and select any one of the following:
    • Sunrise: schedule will be triggered at sunrise.
    • Sunset: schedule will triggered at sunset.
    • Custom: to set the required start/end time (D).
  4. Tap (E) to set the brightness level from the list:
    • Maximum: 100% brightness level.
    • High: 75% brightness level.
    • Medium: 50% brightness level.
    • Low: 25% brightness level.
    • Very Low: 10% brightness level.
  5. Select the days you want to repeat the schedule (F).
  6. Tap Month Repeat (G) to set the months you want to repeat the schedule.
  7. Tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?