DUG_Iconic Dimmer_CLP-00

Switching/Dimming the device using app

Using the Wiser app, you can switch on/off and increase/decrease the brightness of the device.

Switch on/off the device

On the Home page, tap the power button (A) to switch on/off the Dimmer.

TIP: You can also navigate to the control panel of the device and tap to switch on/off the Dimmer. The control panel always shows the current state of the Dimmer.

Adjusting the brightness of the device

To increase/decrease the brightness of the device:

On the Home page, tap ˅ (B) for common function and drag the slider to adjust the brightness of the Dimmer.

TIP: You can also navigate to the control panel of the device and drag the sliding bar up/down to increase/decrease the brightness. The control panel always shows the current brightness percentage of the Dimmer.
NOTE: During timer mode, the dimmer automatically turns off after a specified period of time. Refer timer mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?