DUG_Wiser Micro Module Dimmer_CLP-00

Setting RL-LED mode

You can change the dimming mode in the app if you have problems with light flickering. By changing the dimming mode, the dimming quality is also improved.
To set the RL-LED mode:
  1. On the Home page, Tap All devices > Micromodule Dimmer
  2. Tap Settings.
  3. Tap Dimming Mode and Select Leading Edge (RL-LED) (A) from the slide-up menu.
    NOTE:
    • Refer to Technical Data for more information.

    • Manual operation (Optional): Press the Push button 14 times.

      • If the status LED blinks 3 times in green, RL-LED mode is enabled.

      • If the status LED blinks once in green, Auto mode is enabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?