DUG_Wiser Micro Module Dimmer_CLP-00

Testing the device

Before using the module, manually test the module and make sure that it works when connected to the lighting devices.
  • Short press the push button once, the connected lighting device turns on/off.

  • Press and hold the push button to adjust the dimming level of the connected lighting device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.