990-6290D-001

Connect the Synchronization Cables between Two UPS Systems

Supports synchronization for up to 4+4 parallel systems.

  1. Connect the optional synchronization cables between the UPS systems.

    For Two Single UPS Systems

    For Two Parallel UPS Systems

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.