990-6290D-001

Final Installation

  1. Reinstall the protection cover in front of the non-Class 2/non-SELV terminals.
  2. Reinstall the signal cable cover.
  3. Reinstall the protection cover.
  4. Reinstall the upper plate.
  5. Reinstall the lower plate.
  6. Install the kick plates:
    NOTE: The kick plate parts are delivered in the UPS packaging.
    1. Install the two brackets on the right and left front feet.
    2. Install the rear kick plate.
    3. Install the side kick plates.
    4. Install the front kick plate.
  7. Close the doors.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.