990-6290D-001

Communication Interfaces

  1. Slot for optional cold start button

  2. Network management card (NMC)

  3. Dry contacts

  4. Auxiliary contacts

  5. Parallel ports

  6. Load Bus Synchronization port

  7. Remote EPO

  8. RS485

  9. Battery temperature sensor terminal*

  10. Ambient temperature sensor terminal (internal use)

  11. CAN_R: CAN termination resistor

  12. USB port (for service)

  13. Display port (internal use)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.