Battery Safety
|  DANGER | 
|---|
| hazard of electric shock, explosion or arc flash 
 Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| Hazard of electric shock, explosion, or arc flash Batteries can present a risk of electric shock and high
                        short-circuit current. The following precautions must be observed
                        when working on batteries
                         
 Failure to follow these instructions will result in death or serious injury. | 
|  DANGER | 
|---|
| Hazard of electric shock, explosion, or arc flash When replacing batteries, always replace with the same
                        type and number of batteries or battery packs. Refer to the label
                        in the classic battery cabinet for information on batteries in your
                        system. Failure to follow these instructions will result in death or serious injury. | 
|  CAUTION | 
|---|
| risk of equipment damage 
 Failure to follow these instructions can result in injury or equipment damage. |