990-5993C-001

Connect Cables between the Easy UPS 3M and the Modular Battery Cabinet

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not use the cables provided with the modular battery cabinet for installation with the Easy UPS 3M, but use the cable kit E3MOPT006.
Failure to follow these instructions will result in death or serious injury.
NOTE: Route the signal cables separately from the power cables.
  1. Remove the conduit box from the rear side of the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  2. Rotate the conduit box and install.
  3. Remove the right or left side panel.

    Front View of the Modular Battery Cabinet

  4. Connect the battery cables (optional kit E3MOPT006) to the busbars.

    Right Side View of the Modular Battery Cabinet

  5. If more than one modular battery cabinet is part of the installation, connect the battery cables (kit E3MOPT006) between the modular battery cabinets.
  6. Reinstall the side panel.
  7. Fasten the cables to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?