990-5993C-001

Specifications

DANGER
hazard of electric shock, explosion, or arc flash
The modular battery cabinet must only be used with the Easy UPS 3S with internal batteries.
Failure to follow these instructions will result in death or serious injury.
NOTICE
hazard of equipment damage
Refer to the UPS installation manual for detailed specifications for the UPS system.
Failure to follow these instructions can result in equipment damage.
  Easy UPS 3S Easy UPS 3M
Nominal battery voltage (V) 480 for 400 V systems 240 for 208 V systems 480
Battery type Lead-acid Lead-acid Lead-acid
Number of blocks per string 40 20 40
Maximum short-circuit level (ICW) 10 kA 10 kA 10 kA
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?