Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
|  DANGER | 
|---|
| DANGER indicates a hazardous situation which, if
                        not avoided, will result in death or serious injury. Failure to follow these instructions will result in death or serious injury. | 
|  WARNING | 
|---|
| WARNING indicates a hazardous situation which,
                        if not avoided, could result in death or serious injury. Failure to follow these instructions can result in death, serious injury, or equipment
                        damage. | 
|  CAUTION | 
|---|
| CAUTION indicates a hazardous situation which,
                        if not avoided, could result in minor or moderate injury. Failure to follow these instructions can result in injury or equipment damage. | 
| NOTICE | 
|---|
| NOTICE is used to address practices not related
                        to physical injury. The safety alert symbol shall not be used with
                        this type of safety message. Failure to follow these instructions can result in equipment damage. | 
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.