990-5993C-001

Remove the Modular Battery Cabinet from the Pallet

  1. Move the modular battery cabinet to the final installation area using a forklift.
  2. Remove the ramp from the pallet and remove the shipping material.
  3. Place the ramp in front of the pallet.
  4. Loosen the bolts and remove the shipping brackets. Dispose of the shipping brackets.
  5. Roll the modular battery cabinet down from the pallet.
  6. Move the modular battery cabinet to its installation location and use a wrench to lower the levelling feet. Ensure that the cabinet is level.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?