Connect the Power Cables in a Top Cable Entry System
  DANGER | 
               
|---|
| 
                      Hazard of electric shock, explosion, or arc flash 
                     Perform a total power off of the UPS system before connecting
                        the battery cables to the battery breaker. 
                     Failure to follow these instructions will result in death or serious injury. 
                   | 
               
- Lockout/Tagout the breaker in the OFF position.
 - Connect the PE cable.
 - Connect the DC cables (DC+, DC-) from the UPS.
 - Install the protection cover over the terminals on the left side of the battery breaker.
 - Install the batteries as described in the installation manual supplied with the empty battery cabinet.
 - Connect the battery cables (Batt+, Batt-) from the batteries in the empty battery cabinet 1 to the battery breaker.
 - Only for installation with two empty battery cabinets: Connect the ground cable from empty battery cabinet 1 to empty battery cabinet 2.
 - Only for installation with two empty battery cabinets: Connect the battery cables (Batt+, Batt-) from the batteries in
                  empty battery cabinet 2 to the battery breaker.NOTE: Leave a wiring diagram with battery information on site.
 - Install the protection cover over the terminals on the right side of the battery breaker.
 
 DANGER