990-91190B-001

Specifications for 400 V Systems

Maximum Input Short-Circuit Withstand

The maximum input short-circuit withstand for the parallel maintenance bypass panel is ICC=10 kA.

Recommended Cable Sizes

Cable sizes in this manual are based on the minimum requirements in table B.52.3 and table B.52.5 of IEC 60364-5-52 with the following assertions:

  • 90 °C conductors

  • An ambient temperature of 30 °C

  • Use of copper conductors

  • PE cable size is based on table 54.2 of IEC 60364-5-54

  • Installation method C

  • Specific to AC cables: Maximum length 70 m with a line voltage drop <3% installed on perforated cable trays, XLPE-type insulation, single layer trefoil formation, THDI between 15% and 33%.

NOTE: If the ambient temperature is greater than 30 °C, larger conductors are to be selected in accordance with the correction factors of the IEC.

UPS Cable Cable Size per Phase (mm²)
10 kVA UPS 1 Output/UPS 2 output Refer to the UPS installation manual.
System input 16
System output 16
PE 10
15 kVA UPS 1 Output/UPS 2 output Refer to the UPS installation manual.
System input 16
System output 16
PE 10
20 kVA UPS 1 Output/UPS 2 output Refer to the UPS installation manual.
System input 25
System output 25
PE 10
30 kVA UPS 1 Output/UPS 2 output Refer to the UPS installation manual.
System input 35
System output 35
PE 16
40 kVA UPS 1 Output/UPS 2 output Refer to the UPS installation manual.
System input 50
System output 50
PE 16
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.