990-66230B-001

Configure the UPS Bypass

NOTE: This configuration is mandatory for correct UPS operation.
  1. From the main menu, tap Configuration > Bypass.
    1. Set Maximum threshold of bypass voltage to +10%, +15%, +20%, or +25%, default is +10%.
    2. Set Minimum threshold of bypass voltage to -10%, -15%, -20%, -30%, or -40%, default is -10%.
    3. Set Bypass frequency limit to +/-1 Hz, +/-3 Hz, or +/-5 Hz, default is +/-3 Hz.
  2. Tap OK to save your settings.