990-66230B-001

Turn the Inverter OFF

  1. From the main menu, tap Control > Inverter > Inverter off.
  2. Tap OK on the confirmation screen.
  3. If bypass is out of tolerance, a pop-up warning will show on the display. Click OK to transfer with break or click No to stay in inverter operation.