990-66230B-001

Connect the Temperature Sensor Kit (Option)

NOTE: Use the optional temperature sensor kit (E3SOPT003) for this procedure.
  1. Connect the temperature sensor kit to the terminal J3-5/6 (for ambient temperature measurement) or J4-1/2 (for battery temperature measurement) in the dry contacts. See the UPS installation manual for details.
  2. To see the temperature measurements, tap Status > Temperature.