990-66230B-001

Transfer the UPS from Normal Operation to Static Bypass Operation

  1. From the main menu, tap Control > Operation mode > Transfer to bypass operation.
  2. Tap OK on the confirmation screen.
  3. If bypass is out of tolerance, a pop-up warning will show on the display.
    NOTE: It is not allowed to be transferred to bypass operation mode. If you still want to transfer to bypass operation mode with break, refer to Turn the Inverter OFF.