Export UPS Event Logs to a USB Device
Pre-condition:
-
Insert a USB flash drive (preferably less than 16 GB) in the computer, find the USB flash drive in This PC window, right-click and select Format, configure the file system as FAT32, 4096 bytes of allocation unit size, check .
NOTE: It is recommended to use a USB 2.0 flash drive, because USB 3.0 may not support the FAT32 format.
- From the main menu, select .
- Remove the cover for the USB port.
- Insert your USB device in the USB port on the display.
- On the display, tap Export. When
the display shows the message Confirm to export UPS event
logs, tap OK to start the export
process. NOTE: Do not remove the USB device until the export process has finished.
- The display will show the completion status with the message Event dump successful or Event dump unsuccessful. Tap OK to proceed.
- Send the UPS event logs to Schneider Electric customer support.